2. Passive Components
  3. Capacitors

Electrolytic Capacitors

Click here to compare
arrow_down Compare
Description Unit Price
Unit Pack
Stock Info
RUBYCON
RUBYCON 35PJV56MSPA6.3X6.1

35PJV56MSPA6.3X6.1

PJV 56uF 35V 20% 6x6 Part No.: KEL23868 Packaging: REEL PLAST
Unit Price
0.2465 $
Unit Pack
1000
Stock Info
38 weeks
On request
Price, Lead time Datasheet
RUBYCON
RUBYCON 35PJV56M6.3X6.1

35PJV56M6.3X6.1

PJV 56uF 35V 20% 6x6 Part No.: KEL23636 Packaging: REEL
Unit Price
0.2465 $
Unit Pack
1000
Stock Info
38 weeks
On request
Price, Lead time Datasheet
  • «      
  • 1      
  • 2      
  • 3   
41 - 42 of 42 parts

Electrolytic Capacitors - More information

Electrolytic capacitors, also known as "Elkos," are essential components in electronics due to their high capacitance and low cost. They consist of an anode typically made from aluminum or tantalum and a cathode formed by an electrolyte. Electrolytic capacitors differ fundamentally from other types of capacitors like ceramic or film capacitors, as they offer higher capacitance in a smaller size.

The development of electrolytic capacitors began in the early 20th century and has continuously evolved since then. Today, they are used in a variety of fields, including power supplies, energy storage, audio amplifiers, and communication devices. Their importance in modern electronics is undeniable, as they are found in almost every electronic circuit.

Structure and Functionality of Electrolytic Capacitors

An electrolytic capacitor comprises three main components: the anode, the cathode, and the electrolyte. The anode is formed by a metal foil coated with an insulating oxide layer. The cathode consists of a conductive electrolyte, which can be either liquid or solid. The electrolyte plays a crucial role in the capacitor's function, acting as a conductor between the anode and the cathode.

Aluminum and tantalum electrolytic capacitors are the two most common types. Aluminum capacitors are known for their high capacitance and low cost, while tantalum electrolytic capacitors are preferred for their high reliability and stability. The geometry of the capacitor, including the size and arrangement of the electrodes, also affects the component's performance.

Oxide Layer and Its Importance

The oxide layer is central to the function of an electrolytic capacitor. It forms the dielectric barrier between the anode and cathode, determining the capacitance and voltage of the capacitor. Processes for optimizing the oxide layer, such as anodic oxidation, contribute to improving the capacitor's performance and reliability.

Electrical Properties and Parameters of Elkos

The capacitance of an electrolytic capacitor is measured in farads (F) and indicates how much charge the capacitor can store. Another important parameter is the voltage the capacitor can withstand before failing, known as the rated voltage. Impedance and ESR (Equivalent Series Resistance) are also crucial as they affect the energy loss in the capacitor.
Leakage current and dielectric losses are undesirable properties that reduce a capacitor's efficiency. The temperature coefficient and operating temperature range are also important as they determine the capacitor's performance under different conditions. The lifespan of an electrolytic capacitor is influenced by various factors, including operating temperature and the voltage applied to the capacitor.

Rated Voltage and Leakage Current

The rated voltage of an electrolytic capacitor indicates the maximum voltage the capacitor can safely operate at. The leakage current that remains after charging and discharging the capacitor can affect its performance. Careful selection and testing of the rated voltage and leakage current are crucial for optimal capacitor performance.

Advantages and Disadvantages of Electrolytic Capacitors

Electrolytic capacitors offer several outstanding advantages, making them indispensable for various applications. One of the greatest advantages is their high capacitance, enabling them to store and release large amounts of energy. This makes them ideal for applications like smoothing DC voltages, where they balance voltage fluctuations and ensure a stable output voltage. Additionally, electrolytic capacitors are relatively inexpensive to manufacture, making them an economical choice for many electronic devices.

Another advantage is their ability to handle large currents, needed in high-power applications. This is particularly useful in power supplies, where they help reduce ripple current and improve the system's overall efficiency. Electrolytic capacitors also have good temperature resistance and can operate over a wide temperature range, expanding their usability. However, electrolytic capacitors also have some disadvantages. One of the most significant is their limited lifespan caused by the electrolyte. Over time, the electrolyte can dry out or decompose, reducing the capacitor's capacitance and performance. This leads to a higher failure rate and can cause problems in critical applications. Additionally, electrolytic capacitors are polarized, meaning they can only be operated in a specific direction. Incorrect polarity can cause damage or even capacitor failure.

Compared to other capacitor types, such as ceramic or film capacitors, electrolytic capacitors offer higher capacitance but are less stable and have a shorter lifespan. Ceramic capacitors, for example, are not polarized and have very high stability but are limited in their capacitance. Film capacitors provide excellent long-term stability and reliability but are typically more expensive and larger than electrolytic capacitors. In specific applications like audio amplifiers or energy storage systems, electrolytic capacitors are still superior due to their specific properties and provide the required capacitance and performance.

Applications and Uses of Electrolytic Capacitors

Electrolytic capacitors are found in a variety of applications that utilize their specific properties and advantages. In power supplies, they smooth DC voltages and stabilize the output voltage. This function is crucial to ensure a constant and interference-free supply of electronic devices. They help minimize voltage fluctuations and ensure consistent performance, which is particularly important in sensitive electronic devices.

In audio amplifiers, electrolytic capacitors are used to decouple and filter signals. They improve sound quality by eliminating unwanted frequencies and disturbances. This results in clearer and more precise audio signals, essential for high-quality audio components. Additionally, they are integrated into speaker crossovers, helping to separate and distribute different frequency ranges efficiently.

In computers and communication devices, electrolytic capacitors play a central role in energy storage and buffering. They allow short-term power peaks to be absorbed and keep the power supply stable, which is crucial for the operation of processors and other critical components. Furthermore, they are used in specialized applications like medical devices, where their high capacitance and reliability are advantageous. In medical devices that require precise and reliable power supply, electrolytic capacitors ensure stable performance.

Other areas of application include the automotive industry, where they are used in control units and sensor systems, as well as in renewable energy systems, where they help store and regulate energy from solar and wind power systems. Their versatility and performance make them indispensable components in modern electronics.

Selection and Sizing of Electrolytic Capacitors

The selection and sizing of electrolytic capacitors require careful consideration to ensure the best performance and reliability. Several criteria must be considered when selecting an electrolytic capacitor, including capacitance, voltage, and ESR (Equivalent Series Resistance). Capacitance, measured in farads (F), determines how much charge the capacitor can store. The required capacitance can be calculated based on the specific circuit requirements, taking into account factors like voltage fluctuations and load conditions.

The rated voltage is another crucial parameter, indicating the maximum voltage the capacitor can withstand. It is important to choose a capacitor whose rated voltage exceeds the maximum expected operating voltage to ensure long life and reliability. ESR affects the capacitor's efficiency and should be as low as possible to minimize energy losses and reduce heat generation.

Selecting the right form factor and size is also crucial to ensure the best performance. Smaller form factors are generally more space-saving but may have higher ESR values. The ambient temperature significantly affects the capacitor's performance and lifespan, so this factor should be considered in the selection process. High temperatures can shorten the electrolyte's lifespan and increase the failure rate. Recommendations for typical applications help find the right capacitor for specific requirements.

It is also important to consider the capacitor's tolerances and temperature coefficient, as these parameters affect stability and reliability in various operating environments. Selecting a capacitor with suitable specifications for the specific application contributes significantly to optimizing the circuit and avoiding failures. Through careful sizing and selection, the advantages of electrolytic capacitors can be fully exploited, and their disadvantages minimized.

Manufacturing Process and Quality Control

The manufacturing process of an electrolytic capacitor involves several steps, from producing the anode, applying the oxide layer, to final testing. Material selection is crucial for the capacitor's quality and performance. Typical errors during the manufacturing process can be minimized through careful quality control and testing procedures.

Standards and norms play an important role in ensuring the quality and reliability of electrolytic capacitors. By adhering to these standards, manufacturers can ensure that their products meet customers' requirements.

Trends and Innovations in Electrolytic Capacitor Technology

The technology of electrolytic capacitors is constantly evolving. New materials and technologies enable higher capacitance and longer lifespans. Miniaturization is another important trend, allowing for increasingly smaller and more powerful capacitors to be developed.

Environmentally friendly alternatives and recycling methods are also gaining importance as the industry strives to develop more sustainable products. The future of electrolytic capacitor technology looks promising, with continuous improvements and new applications further enhancing the performance and reliability of these crucial components.

Reliable Supply from Rutronik

Whether electrolytic capacitors, tantalum capacitors, film capacitors, or other capacitors: with over 25% supply share, passive components are one of the pillars of our supply chain. Here, smooth delivery is crucial. Many part numbers with high delivery volumes but comparatively low turnover are prone to errors and a logistical challenge. We stand out here with special logistics systems and IT connections.

We understand the importance of quality and reliability in electronic components and are your ideal partner for electrolytic capacitors. With our deep understanding of specific application requirements and commitment to technological excellence, we are ready to support you with all your needs.